Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why doesn't the Debug tab on Control Expert appear for an X80 IO module?

The debug screen will become available when there is a fault on a X80 output module. Establish an online connection with the PLC using Control Expert and navigate to the module ‘s configuration screen. Note, this screen is only available when the output module is mounted on the local CPU rack. It will not display when mounted on a remote IO (RIO) rack.

Similarly, debug screens are not available for Analog modules in RIO racks, so the parameters (Alignment, Filter, Offset...) can’t be changed while online. The debug screen is available when the module is mounted on the local CPU rack.

Debug

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings