Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can PME control Modbus TCP points?

Issue

Customer would like to control a Modbus TCP points to indicate general status of the system in Power Monitoring Expert (PME).

Resolution

As of now PME is not being used to control actions, only read and view. If the customer needs to control the device points such as beaker ON/OFF, they need to opt for EcoStruxure Power Operation.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings