Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
New BMXNOR0200H Web Page Access is Disabled

Issue:

How to Enable BMXNOR0200H Web Access

Product Line:

BMXNOR0200H

Control Expert

Resolution:

By default the Web Access in BMXNOR0200H is disabled due to Cyber Security Requirement and you have to use Control Expert 14. x onwards to Enable the Web Access please follow the below steps ,

Step1: Try to Configure a Dummy application using Control Expert & Enable the Web Access in Security settings  and save the application as .STA

Step2: Please Open the .STA file without doing a build & download it to the CPU after which the CPU should have the Web Access

NOTE:

If you want to disable the Web Access then as mentioned in the image these Services can be disabled only on BMXNOR0200H Firmware version V1.7 or higher

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings