Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
BSCM Modbus SL cord extension

Issue:

Regarding the Modbus cable (LV434221 / LV43422 / LV434223). If the customer requires a cable longer than 3m, what is the best solution to recommend?

Product:

ComPacT NSX, BSCM Modbus SL cord

Solution:

Customer can use TRV00870 to extend RJ45<>RJ45, the maximum recommended length is 10 meters between BSCM+ and Modbus Hub, Example the sequence is LV434223 to TRV00870 to ULP CABLE to Modbus hub.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings