Control Expert DTM Backward Compatibility
Issue:
Control Expert DTM backward Compatibility .
Product Line:
Control Expert 14.x to higher
Unity Pro 13.x to lower.
Resolution:
DTMs may not be backward compatible. If an application created with Unity Pro/EcoStruxure Control Expert contains DTM version n, do not open and run DTM of version n-1 (or earlier).
DTMs are generally forward compatible. If an application created with Unity Pro/EcoStruxure Control Expert contains DTMs version n, it can be opened and run with DTM version n+1 and above.
As some modules and controller families comes with a DTM (M580 controller, 140CRP312, 140NOC77•, TSXETC101, BMXNOC, BMENOC, 140NOC, HART, PME SW...) this means for example:
-
An M580 application created with Unity Pro V8.1 cannot be built with Unity Pro V8.0.
-
An M340 application with BMXNOC created with Unity Pro V8.1 cannot be built with Unity Pro V8.0.
Released for: Schneider Electric Australia
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.