How can we help you today?

Are M580 BMECRA***** Ethernet Controllers compatible with BMXXBP**** X-Bus Backplanes?

Question

Can M580 controllers with an Ethernet bus port on the back connect to an X-bus backplane?

Affected Products

  • M580 BMECRA*****
  • M580 BMXCRA*****
  • Backplane BMEXBP****
  • Backplane BMXXBP****

Answer

Simply put, the answer is no.

Ethernet controllers and X-bus backplanes are not compatible, neither are X-bus controllers and Ethernet backplanes. The bus technology between the bus port on the back of the controller and the bus technology within the backplane must match. i.e. BMXXBP****with BMXCRA***** and BMEXBP**** with BMECRA*****.

There is a mistake within the Modicon M580 RIO Modules Installation and Configuration Guide (12/2023) that indicates, otherwise. I would like to reenforce, this is a mistake within the documentation. Please refer to the Modicon M580 Catalog (12/2024) for tested compatibilities.

Please be Aware

This FAQ was written 07/2025. The documents linked above may be updated, replaced or removed by the time you are reading this. Please check the product page for current documentation on any Schneider Electric products.

Schneider Electric Australia
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
Start your sales inquiry online and an expert will connect with you.
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings