How can we help you today?

How to Auto Start Windows pre-installed Runtime HMI (HMIG5U ,HMIG5U22, HMIGTW7353 ,..etc) after Power Cycle

Issue:

After downloading the Project file to Windows pre-installing Runtime HMI , power cycle the HMI and its asking

Vijeo-Designer Runtime

If I click in “Continue” is running the application , but shouldn’t it be automatic?

Product Line:

HMIG5U/HMIG5U2/HMIG5U22/HMIGTW7353 .

Resolution:

Please Click on "Lock" in the above image and restarting the HMI will enable the Write Filter ,then the Target Runtime will Start Automatically.

NOTE:

If you want to Shut down the Vijeo Runtime that is running automatically after Power-up , then Please use an External Keyboard and press Alt + Ctrl + Delete ,and then go to Task Manager to Close the Vijeo Runtime .

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings