Troubleshooting 3rd Party Meter Communication Issues in EVCE Webpage
Issue Summary:
The third-party meter status is showing a red cross on the EVCE webpage, signifying that there is no communication between the LMS and the meter.
Product Line:
- EcoStruxure EV Charging Expert (EVCE),
- Panel Server Universal (PAS600L),
- 3rd Party Meter
Environment:
- 3rd Party Meter (Crompton SL1-01), PAS600L, and LMS
Resolution:
Verify the IP address and slave address in the EVCE webpage.
- IP address should be that of the PAS600L.
- Slave address must match the meter’s configuration.
Check the custom meter settings in EVCE Webpage.
- Some meters may require register offsets (e.g., offset by 1).
Use a Modbus tool or the PAS600L webpage to read meter data.
- If data is visible, the meter and PAS600L are communicating correctly.
Confirm both the LMS and PAS600L are on the same network.
- Try pinging both IP addresses.
Disable DHCP client and manually set IP address, subnet mask, and gateway.
Released for: Schneider Electric Australia
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.