Com'X 200 is inaccessible from Browser
Issue
My Com'X 200 is inaccessible from a web browser. The gateway itself is still functioning as gateways and pulse inputs.
Resolution
There is possibility that the Com'X is not on the latest Firmware Version. The latest firmware version for the Com'X 200 is version 3.5.54.
https://www.se.com/au/en/download/document/ComX200_v3.5.54/
Depending on the Firmware Version you are on, you may need to upgrade to firmware version 2.1 first.
https://www.se.com/au/en/download/document/ComX210v2-1-18_Firmware_EBX210/
After that you can upgrade to firmware version 3.5.54.
Note: Firmware Version 3.5.54 is the final firmware version that is available for for the ComX 200. As there is limited to no support for the ComX 200, if the firmware upgrade does not assist with the Communication issue you may have to move to a different product like Panel Server.
Released for: Schneider Electric Australia
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.