How can we help you today?

For the BMEAHI0812, if not using HART functionality, is it possible to set up the module without adding a device to the DTM browser?

It is possible by navigating to the CPU's DTM (in the DTM browser) and adding the IP address and DHCP identifier of the BMEAHI0812 module in the "Manually Added Devices" section.

DTM

Once the applicable Analog channels are enabled and the module receives its IP address from the CPU, the analog input signal data will be read as per normal.

Schneider Electric Australia
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
Start your sales inquiry online and an expert will connect with you.
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings