Ecostruxure Machine Expert Showing Untrusted Digital Signature
Issue:
Ecostruxure Machine Expert doesn’t work as normal ,after a Windows Update and keeps on getting the following message ,
Product Line:
Ecostruxure Machine Expert
Resolution:
The integrity check was triggered by new Signed Certificates related to the Windows update.
This has no effect on the used applications , if you Click the "Continue using Netmanage Server".
Till Machine Expert V2.3 this will be triggered because the new certificates are not in our whitelist and from Machine Expert V2.3 this issue will not be present.
For versions before V2.3, the integrity check could be silenced (e.g. LogicBuilder "C:\Program Files\Schneider Electric\EcoStruxure Machine Expert\V2.2\LogicBuilder.exe" --SignatureVerificationWarningLevel=Silent) for ESME or other tools like Diagnostics, Controller Assistant and also Netmanage, see also
https://product-help.schneider-electric.com/Machine Expert/V2.2/en/SoMProg/index.htm#t=SoMProg/D-SE-0108425.html
But if Netmanage is not running as a Windows Service, then you have to uninstall the Windows-Service and Start manually to start Netmanage in silent mode until Machine Expert V2.3
From ESME V2.3 it's also possible to run the Netmanage service in silent mode by setting the Config file
Released for: Schneider Electric Australia
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.