Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In a Modicon DRS switch, is it possible to obtain status data via Ethernet/IP without overwriting any parameters configured via the web interface?

Yes it is possible, as long as the EIP connection is changed to Input Only. By default, it is set to Exclusive owner, so when there is an EIP connection to the switch, the output data will override what is selected on the webpages. Please see example from M580 PLC DTM browser below.

DTM browser

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings