Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How should the reference speed be configured for an ATV320 Solar drive that is powered only by a solar panel and needs to operate at the maximum possible speed?

Question:

How should the reference speed be configured for an ATV320 Solar drive that is powered only by a solar panel and needs to operate at the maximum possible speed?

Answer:

Method 1:

Set maximum speed reference via terminal AI1:

AI1=10V

Method 2:

Configure LSP (Low Speed) = HSP (High Speed):

LSP=HSP

The drive’s integrated MPPT (Maximum Power Point Tracking) algorithm will then automatically adjust the motor speed based on the available solar energy.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings