How can we help you today?

The breaking capacity and operating time of the Acti9 iMX+OF shunt trip release module (Ref: A9A26946).

Issue:

What is the breaking capacity and operating time of the Acti9 iMX+OF shunt trip release module (Ref: A9A26946)?

Product Line:

Acti9 iMX+OF Auxiliary Trip Units

Environment:

Used with Acti9 circuit breakers (e.g., iC60, iC65) for remote tripping applications.

Resolution:

Breaking Capacity:

The A9A26946 module does not have its own breaking capacity because it is not a circuit breaker. It operates in conjunction with the associated protection device (e.g., Acti9 iC60/iC65), which determines the system’s breaking capacity.

Operating Time:

• Depends on the control voltage applied.

• For a sudden voltage application (0 → 100% of Un), the iMX operating time can be <10 ms.

• Combined with the associated circuit breaker, the total power circuit breaking time can be approximately <18 ms.

For detailed specifications, refer to Global Module CA908029E.

Schneider Electric Australia
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
Start your sales inquiry online and an expert will connect with you.
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings