How can we help you today?

Where are the sysParameters of TM173 documented ? The term sysParameter is not mentioned in either the M173 Hardware Guide or the EcoStruxure Machine Expert - HVAC Operating (Programming) Guide.

Issue:

Where are the sysParameters of TM173 documented ? The term sysParameter is not mentioned in either the M173 Hardware Guide or the EcoStruxure Machine Expert - HVAC  Operating (Programming) Guide.

Product Line:

TM173 Product Line

Resolution:

Target variables are not documented in the Hardware guide, they are described in the variable properties.

sysParameter is a struct of type sysParamStruct:

Properties_Window_1

You can find its description in the Struct definition:

Properties_Window_2

You can Read/Write a struct using the IEC standard language sysParameter.<fieldname> := <value>;

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings