Hoe kunnen wij u vandaag helpen?

What is the contact rating of the 9999SX11 and 9999SX12?

Issue:
Where can I find the contact rating of part #s 9999SX11 and 9999SX12.

Product Line:
8502 Contactors and 8536 Starters

Environment:
NEMA Contactors and Starters

Resolution:
These contacts are designed for AC applications only. The following ratings are based on 35% power factor and voltage specific.

120 volts or less = 30 amp make, 3 amp continuous, 3 amp break.
120 to 600 volts = 3600 VA make, 3 amp continuous, 360 VA break.