Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
What is the NEMA rating for the XACA pendant station enclosure?
Issue:
NEMA Rating of the XACA Pendant Station

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony XAC Medium-Duty Pendant Stations

Resolution:
It is rated NEMA 4, 4X (indoor and outdoor), and IP65.
Pistol grip NEMA 4, 4X (indoor), and IP65.