Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
When do the cooling fans on the ATV212 drives come on?
Issue:
When should the cooling fans on the ATV212 drives be running?

Product Line:
Altivar 212

Environment:
All

Cause:
Fan control strategy

Resolution:
The fan starts when the drive is in RUN state.
The fan stops after the STOP command (with a time delay in relation to the thermal state).