Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
How to wire start stop on the ATV61 or ATV71 drives?
Issue:
Wiring a start stop pushbutton or a dry contact on ATV61 or ATV71.

Product line:
ATV61 and ATV71

Environment:
All models, all serial numbers

Cause:
Wiring

Resolution:
In 2-wire control, wire the start/stop contact between +24 and L11.
In 3-wire control, the normally closed Stop pushbutton is wired between +24 and LI1. The normally open Start pushbutton is wired between +24 and LI2.