Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Does the ATV61/71 jog function require a run command to work?
Issue:
Jog function requirements on ATV61/71

Product Line:
Altivar 61/71

Environment:
All models and serial numbers

Cause:
The Jog will not start when the assigned logic input goes high.

Resolution:
When the JOG function is activated, the VFD still needs a run command input to run the motor.