Hoe kunnen wij u vandaag helpen?

Video: How to lock/unlock the ATV212 drive?

Issue:
ATV212 to be locked so that parameters can not be altered.

Product Line:
Altivar 212  ATV212

Environment:
Drive parameters

Cause:
n/a

Resolution:
Press MODE to AUF
Arrow down to F--- and enter.
Go up to F700.
F700 = 0 is unlocked.
F700 = 1 is locked.

The drive will not allow any programming changes unless this parameter is set to 0.



If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)