Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
How many simultaneous Webreach Connections can access the Server?

For non-server operating systems (IE: WinXP) 10 Webreach connections can be gathering data.
For Server Class operating systems (IE: Windows Server 2003) the number of connections is only limited to BandWidth. So effectively unlimited connections can be made.

Original article#16715

Last Revised: May 29 2007

Public

All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL186620 V1.0, Originally authored by KBAdPM on 07/06/2007, Last Edited by KBAdPM on 07/06/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0, ION Enterprise V4.5