How is the ATV12 programmed for a 4-20mA analog input on AI1?
Issue:
ATV12 programming AI1 for a 4-20mA analog input.
Product Line:
Altivar 12
Environment:
All models
Cause:
AI1 factory default is for a 0-5Vdc input.
Resolution:
Navigate to the AI1 Config menu using path ConF-FULL-IO-AI1-. Set AI1t = 0A. The input range is factory defaulted to 4-20mA, but can be changed with parameters CrL1 min and CrH1 max.
Gepubliceerd voor: Schneider Electric Belgium