Populaire vragen (FAQ's) zoeken
Where can I download the EDS files for the Ethernet IP, Devicenet, CANopen, or EtherCAT?
Issue:
Where can I download the EDS files for the Ethernet IP card?
Product Line:
ATV61, ATV71, ATV32, ATV Process
Environment:
All
Resolution:
Use this link to access the Global website where EDS files are available for download. Be sure to download the EDS file that matches your Drive and Product Version.
https://www.se.com/us/en/download/search/?docTypeGroup=3587139-Software%2FFirmware&docType=1555901-EDS+Files
You will need to find out your drive's product version to choose the correct EDS file.
Example: In the ATV61 or ATV71; go to menu 1.11 in the drives menu enter
find the product Vxxxxxxxxx
This product version will need to be the version of the EDS file you download for that specific drive.