Hoe kunnen wij u vandaag helpen?

why can't I connect to the CPU using Unity Pro or Control expert ?

A BMXXBE module (rack extension module) may be installed, without an extension rack connected.
remove the xbe module from the local rack, or add an extension rack.