Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
How to disable the input phase loss detection on an ATV312 drive?
Issue:
Single phase power and disabling input phase loss.

Product Line:
ATV312

Environment:
Only accessible on 3 phase drives
ATV312H...M3 and ATV312H...N4

Cause:
With single phase power supply, the VFD trips PHF.

Resolution:
Enter and scroll down to FLT-.
Enter and scroll down to IPL.  Set it to no.
Note:  The drive state must not be running.