PowerSCADA Expert (PSE) ION Protocol Help File
Setting up/Troubleshooting an ION protocol device in PowerSCADA Expert (PSE).
Product Line:
PowerSCADA Expert 7.30
PowerSCADA Expert 7.40
PowerSCADA Expert 8.0
Environment:
PSE projects with ION protocol devices.
Cause:
Since the ION protocol is newly supported by PSE, it is useful to have a help document that describes how the ION devices communicate and how their tags are addressed.
Resolution:
Attached is the help file for the ION Driver. Some of the key topics that this help file covers are: Configuring Variable Tags, Supported Data Types, .ini Parameters, and Ethergate connections.