Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
I measure an Application Response Time that is higher than I expected.
If the MAST is cyclic, the default RPI is set to 60ms. If the actual execution time of MAST is lower than 120ms, the ART is affected by the RPI.
Adjust the RPI value to your  needs.
Or set your MAST task in periodic mode.