Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
What is the code FLU on the display of the Altivar Drives?
Issue:
FLU on the display of a drive.

Product Line:
Altivar 61
Altivar 71
Altivar 320
Altivar 340
Altivar 930

Environment:
All models

Cause:
N/A

Resolution:
FLU is a VFD state/status.
It is not an error code.
FLU indicates that motor fluxing is in progress.  Review the Programming manual for your drive to identify how to enable or disable Fluxing.