Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
What cable do I use between the Magelis XBTGC2330T DB9 port and an Altivar RJ45 port for Modbus RTU RS485?
Issue:
What cable do I use between the Magelis XBTGC2330T Dsub9 port and an Altivar RJ45 port for Modbus RTU RS485?

Product Line:
XBTGC/GH/GK/GT, Altivar

Environment:
Cable for Modbus Serial Communication

Resolution:
The cable that can be used for this combination of devices for Modbus Serial Communication is the XBTZ9008.