Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Can you program the ATV212 Drive to do an automatic restart after power loss in local control?
Issue:
ATV212 configuration to do an automatic restart after power loss in local control

Product Line:
Altivar ATV212

Environment:
All

Cause:
Running the drive in local mode they need to have the drive restart in the event of loss of power.

Resolution:
The drive can not be programmed to do a automatic restart in local mode. You will need to push the start button again on the face of the drive to start the drive back up.
If you want a automatic restart after power loss consider using 2 wire terminal control instead.