Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Does the TM221 have the capability to do 120vac Inputs and Outputs?
All the TM221's that end with the letter "R" are Relay Outputs and can do 120vac Outputs.
To do 120vac Inputs add a TM3DI8A module to the TM221.