Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Will the VW3G48101 keypad kit for the ATS48 series soft starts work with the ATS46 series soft starts?
Issue:
Can I use the VW3G48101 keypad kit of the ATS48 to connect to the ATS46?

Product Line:
VW3G48101 remote mount keypad kit for use with the ATS48 series starters.

Environment:
All models, All serial numbers.

Cause:
Customer has ATS46 soft starters and needs a remote mount keypad kit.  The kit designed for the ATS46 is obsolete and no longer available.

Resolution:
No.  The VW3G48101 remote mount keypad kit is compatible with ATS48 series soft starters only.  It will not work with the ATS46 series soft starters.