Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
BMXFTW301 cable diameter
Issue
This Resolution provides the maximum diameter for the BMXFTW301 cable.



Product Line
BMXFTW301



Resolution
The maximum BMXFTW301 cable diameter is 9.5mm


The BMXFTW301 is a cable used with M340 I/O modules.  It has a 20 pin terminal block on one end and color-coded flying leads on the other end.