Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
BMXFTW308S cable diameter
Issue
This Resolution explains the maximum diameter for the BMXFTW308S cable.


Product Line
BMXFTW308S


Resolution
The cable diameter is 11.2mm.

The BMXFTW308S cable is a shielded cable used with  the M340 I/O modules.
It has a 28 pin terminal block on one end and color-coded flying leads on the other end.image1