Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
iRIO Modbus Function Code 02, is iRIO able to read Modbus finction code 02 (input status) ?
Yes, it's possible to  configure the modbus function code 02 need  to be configured in the variable address field