Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Does M580 CPU support the CIP service “send RR data”?
Issue

Why is the M580 returning “service not supported “ message?

Product Line

M580, BMENOC

Resolution

M580 supports "Send RR Data" in a successful response to a Forward Open request.

However when configure the M580 as adapter (local slave) to be scanned by a SCADA or Rockwell PLC, the M580 might return a “not supported service” message to the “send RR data” because it doesn’t support Rockwell tags!!