Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
How can you reset a fault in the ATS48 soft start?
Issue:
Fault reset in ATS48

Product line:
ATS48, Altistart 48

Environment:
All

Cause:
Softstart is faulted

Resolution:
Remove the control power (CL1-CL2 voltage) from the unit until the display goes off.  Wait a few seconds and re-apply the control power. This resets the fault.  If the unit powers up to a fault code, it has faulted again.  Investigate the cause of the fault.