Does the ATS48 have a built in Shorting Contactor?
Is the ATS48 built with shorting contactor?
Product Line:
ATS48
Environment:
Shorting contactor
Cause:
n/a
Resolution:
No, the ATS48 does not have a built-in Shorting contactor. But the ATS22 is the only soft start with a built-in Shorting contactor.