Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
What is the maximum number of drives you can daisy chain using Modbus TCP/IP on an ATV32
Issue:
Maximum number of drives to daisy chain

Product Line:
ATV32, ATV61 and ATV71

Environment:
Modbus TCP/IP
Daisy chain part number
ATV32 - VW3A3616
ATV71 or ATV61 - VW3A3310D

Cause:
None

Resolution:
The maximum number of devices is 32.  However, there may be some limitations.  Please see the attached.

Schneider Electric Belgium

bijlage(n)
ATV in Ring or daisy chain topology.pdf [76.25 KB]