Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Is the ATV61HD30N4 NRTL listed?
Issue:
ATV61HD30N4 NRTL.

Product Line:
Altivar 61, Altivar 71, Altivar 312, Altivar 212, Altivar 12, Altivar 31, Altivar 58, Altivar 66, Altivar 630, Altivar 930

Environment:
All Serial numbers

Cause:
Needing NRTL certification

Resolution:
Only by way of UL. The NRTL is a US Government Program. If equipment is either UL or FMRC listed, then it is recognized as NRTL. There is no ``Label`` for NRTL.