Hoe kunnen wij u vandaag helpen?

Are there any MiCOM Relays that have the terminal blocks located in the front of the relay?

Question
Are there any MiCOM Relays that have the terminal blocks located in the front of the relay?

Answer
Issue
Customer is looking for MiCOM Relays that has the terminal blocks in the front of the relay behind the front panel.

Product Line
MiCOM Px38 line

Environment
Ordering


Resolution
Electrical connections are made via plug-in threaded terminal blocks. The threaded terminal blocks in the surface-mounted case are accessible from the front of the device after unscrewing the crosshead screws on the sides (see Figure 4-1, 1) and removing the user interface (HMI). The user interface (HMI) can then be secured by inserting the tabs in the slots in the left side wall (see Figure 4-1, 2). The flush-mounted case is connected at the back of the case.

img1