The stall monitoring current rating is a percentage of which current rating?
Stall monitoring current rating percentage meaning.
Product Line:
Altivar 630 Process Drive
Environment:
All models and serial numbers
Cause:
None
Resolution:
For the ATV630, the [Stall Current] StP2 parameter entered is a percentage of the motor rated current.