Can the SD card in the M340 CPU be accessed via the NOE or NOC using FTP
Can the SD card in the M340 CPU be accessed via the NOE or NOC using FTP
Product Line
M340
Environment
Windows 10
Resolution
The answer is no.
The SD card in the M340 CPU can only be accessed if you are directly connected to the CPU.