Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Can the Altivar drive's freewheel stop function, be use with a normally open contact ?
Issue:
Altivar drive's freewheel stop function assigned for make or break activation.

Product Line:
Altivar

Environment:
ATV61 ATV71 ATV312 ATV12, ATV32

Cause:
Normally open contact close to freewheel

Resolution:
No option in the drive settings to reverse the freewheel logic function.
Assigned logic input, must be active +24vdc (made)  break to trip.