Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
Multimotor configuration ATV630

Article available in these languages: Nederlands

With an ATV630 it is not possible to implement a multi motor configuration with different motors.
Only with equal motors it can be done with parameter set switching ( no motor parameters ! ) to make different application settings for each motor.
This only can be done with ATV930 variable speed drives.
See FAQ  FA300488  for “Multimotor configuration ATV930”