Can the Quantum 140NOE77101 hostname be changed?
Where the Host Name “140-NOE-771-01 Module” is being stored? Can it be changed?
Product Line
Quantum
Resolution
The Host Name “140-NOE-771-01 Module” is stored in the SNMP OID “System Name:” property.
The SNMP OID “System Name:” property is it read only, therefore, the hostname can’t be changed