Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
What can cause High CPU usage on the HMIG5U?
Issue:
What can cause High CPU usage on the HMIG5U?

Product Line:
HMIG5U, HMIG5U2, Magelis iPC

Resolution:
A common cause of high CPU usage on the HMIG5U/HMIG5U2, or Magelis iPC in general, can be attributed to Windows Update running in the background when there is no internet connection. It will constantly try to reach out to the server, even if there is no internet connection. The remedy would be to turn off the Windows Update.