Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
How long can be unshielded cables with IEC60034-25 motorsif ATV630/930 is used?
If the motor fullfil IEC60034-25, unshielded motor cables can be up to 150m without additional filter.