Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Hoe kunnen wij u vandaag helpen?
What is the purpose of internal battery in Pm2225 meter ?

Issue

What is the purpose of the internal battery in the PM2225 meter?

Product Line

PowerLogic™ PM2225 Series Meter.

Environment

Installations where maintaining accurate timekeeping is critical, even during power outages or meter shutdowns.

Resolution

The internal battery in the PM2225 meter keeps its clock running and helps maintain the time even when the meter is powered down.